Configured Administrator Machine

Perform the next steps on the administrator machine you just configured and tested.

  1. Browse to ReplicationConsole.exe.config and copy this file to a shared network directory. This file resides in the ArcFM Solution\Bin directory. This step is necessary for all Mobile Solution implementations.
  2. Browse to Program Files\Miner and Miner\ArcFM Solution\Bin\Xml and copy DatabaseConnections.xml to a shared network directory.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?