Deployment

Now you have saved in a shared network directory all files necessary to deploy your Mobile Solution to any number of client machines. The following steps are performed on these unconfigured client machines. Copy files from the shared network drive to the unconfigured client machines.

  1. Copy the directory structure from your Administrator machine to each field machine. This directory structure must be EXACTLY the same on each field machine as it is on the Administrator machine. For example, if you copy from C:\ReplicationField to D:\ReplicationField, you will experience a number of problems on the field machine.
  2. Copy the DatabaseConnections.xml file from the shared network directory to the Miner and Miner\ArcFM Solution\Bin\Xml directory on the client machine you're configuring.
  3. Copy the ReplicationConsole.exe.config file from the shared network directory to the Miner and Miner\ArcFM Solution\bin directory on the client machine you're configuring. If the file already exists at this location, you may overwrite it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?