Upgrade Session Manager to 8.3.1

Use these upgrade instructions if you are:

  • Using a version of Session Manager older than 8.3.1

  • Upgrading to a version of Session Manager that is 8.3.1 or higher

These instructions are intended for GIS administrators who currently are in production with a previous version of Session Manager and who want to upgrade to the most recent version of the ArcFM Solution. This document does not apply if you are not currently using Session Manager and will be implementing it with the latest release of ArcFM (i.e., you are new to ArcFM and are starting with the current release). If this is the case, refer to Set Up Session Manager.

If you are upgrading your Process Framework, you may also need to use the Process Framework Database Upgrade tool.

Upgrade to 8.3.1

With release 8.3.1, the tools included with ArcFM’s Session Manager were retrofitted to use the new Task/Subtask architecture provided with the Process Framework. Since the tools now depend on new tasks, they will be disabled if the tasks do not exist. All tools in Session Manager are affected by this change.

You will need to create the following tasks using the Process Framework Administration Tool. The Task Name must appear exactly as shown in bold below.

  • Open Session

Node Type: Session

Assign Subtasks: (in order as shown)

  • Open Session

  • Save Session

Node Type: Session

Assign Subtasks: (in order as shown)

  • Does user own session node?

    • Save Session

  • Close Session

Node Type: Session

Assign Subtasks: (in order as shown)

  • Close Session

    • Switch To Parent Version

  • Submit Session

Node Type: Session

Assign Subtasks: (in order as shown)

  • Does user own session node?

    • Submit Session

Mobile Note: If you're setting up this task for use in the field with Mobile, use the Mobile Submit Session subtask instead of the Submit Session subtask.

  • Change Session Owner

Node Type: Session

Assign Subtasks: (in order as shown)

  • Change Session Owner

  • Reject Session

Node Type: Session

Assign Subtasks: (in order as shown)

  • Does user own session node?

    • Reject Session

  • Delete Session

Node Type: Session

Assign Subtasks: (in order as shown)

  • Does user own session node?

    • Delete Session

  • Reconcile Session

Node Type: Session

Assign Subtasks: (in order as shown)

  • Does user own session node?

    • Reconcile Session

  • Post Session

Node Type: Session

Assign Subtasks: (in order as shown)

  • Does user own session node?

    • Post Session

  • Unlock Session

This task is optional.

Node Type: Session

Assign Subtasks: (in order as shown)

  • Unlock Node

  • Create Session

The Create Session task must be created for each filter node in your database.

Node Type: AllSessionsFilter, UserSessionsFilter, UserStatusSessionsFilter, and any other custom filters

Assign Subtasks: (in order as shown)

  • Create Session

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?