Upgrade Session Manager to 9.1

Use these upgrade instructions if you are:

  • Using a version of Session Manager older than 9.1

  • Upgrading to a version of Session Manager that is 9.1 or higher

These instructions are intended for GIS administrators who currently are in production with a previous version of Session Manager and who want to upgrade to the most recent version of the ArcFM Solution. This document does not apply if you are not currently using Session Manager and will be implementing it with the latest release of ArcFM (i.e., you are new to ArcFM and are starting with the current release). If this is the case, refer to Set Up Session Manager.

If you are upgrading your Process Framework, you may also need to use the Process Framework Database Upgrade tool.

Upgrade to 9.1

With release 9.1, tools were added to Session Manager to support the Redliner Extension functionality. The following role and transition are necessary only if you wish to use ArcFM Solution's graphic editing functionality.

Roles

The following must appear in the Roles column exactly as they appear below. Any Role Name may be assigned.

  • SESSION_REDLINE_TECH

Tasks

You will need to create the following task using the Process Framework Administration Tool. The Task Name must appear exactly as shown in bold below.

The following task should be added to the Session Manager database on the Enterprise server (e.g., SessionManager.mdb). If you wish to use the redlining functionality in a mobile environment, add this task to the SessionManager Field.mdb as well.

  • Open Redline Session

Node Type: session

Assign Subtasks: (in order as shown)

  • Open Graphic Session

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?