API Keys Tab

API keys can be thought of as service accounts, which help control non-human logins to various systems. These keys are listed in alphabetical order.

Click here to take it for a test drive.

This opens Solution Center straight to User Management.


Add New API Key

  1. Click the API Keys tab.
  2. Click the Add New button.
  3. Provide a descriptive name and click Add Role. A Select Role window pops up.

  4. Choose one or more roles and click Apply.
  5. After you click Save at the bottom of the window, you are given a Client Secret that is never shown again. If you close the app without noting the Client Secret, there is no retrieving it.

    IMPORTANT:
    • Client IDs should be treated like usernames.

    • Client Secrets must be treated like passwords and never shared with others.

    • The markup integration service must have the following roles assigned:

      • Mobile.Admin

      • Monitoring.Reporter

      • ServiceBus.Configuration.Reader

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?