Workflows

The Dynamic Workflows plugin is your control center for:

  • Viewing the workflow path of a design, task, markup, or other job. These can be in progress or complete.

  • Troubleshooting a workflow error.

  • Modifying existing workflow paths, states, and requirements.

  • Creating new Assignment Types to incorporate into a dynamic workflow.

  • Creating and running test cases to validate workflow expectations.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?