Mapping

On the Mapping tab in the Feeder Services plugin are two sections, Maps and Geodatabase Regions.

  • Maps — From the drop-down, select an operational map to act as your Network Feature Service. Feeder Services uses this map to create and update Geodatabase Regions (GRRs), and inform the application of your low voltage (LV) subnetworks to group within the GRR. Refer to Choose an Operational Map in the Feeder Services implementation guide.

  • Geodatabase Regions (GRRs) — Click the Edit icon to group LV subnetworks together in the same GRR export, rather than export them into separate GRRs. Refer to Create Geodatabase Regions in the Feeder Services implementation guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?