Markup Settings

The credentials are used for machine-to-machine communication when markup is trying to communicate with ArcGIS Server to send and receive markups.

IMPORTANT: Create a Portal account for these machine-to-machine communications. Additionally:
  • The Portal account can be the same for Sync Settings and Markup Settings. Or, for more granular access control, use a separate Portal account for Sync Settings and Markup Settings.

  • For Markup Settings, the Portal account must have access to all Markup feature services.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?