Logs

Administrators often use the on-prem Edge Service log files to diagnose problems. The same is true for the Hosted Edge, but because it is hosted, you do not have direct access to the logs. Instead, you can find diagnostic logs in Solution Center in the Feeder Services plugin on the Logs tab. Refer to Logs for the Hosted Edge in the Feeder Services implementation guide for more information.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?