Sync Settings

The credentials are used for machine-to-machine communication when sync is trying to communicate with ArcGIS Server to generate replicas and deltas.

IMPORTANT: Create a Portal account for these machine-to-machine communications. Additionally:
  • The Portal account can be the same for Sync Settings and Markup Settings. Or, for more granular access control, use a separate Portal account for Sync Settings and Markup Settings.

  • For Sync Settings, the Portal account must have access to all map services that require offline data.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?