Introduction

The ArcFM Solution Center is the nucleus for configuring settings of all ArcFM XI applications. It helps you:

  • Manage users

  • Create Session Manager sessions

  • Configure operational maps, reference maps, and basemaps to be used in your applications

  • Monitor services and incidents

  • Manage offline replicas and tile packages

The following para publishes only for Mobile. AShively 6/10/19
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?