DOCA0186EN-02

Front Face Description

Front Face

The main controls, operation indicators, settings, and locking mechanisms are on the front of an electrically operated circuit breaker (with motor mechanism).

  1. Faceplate

  2. Charging handle

  3. Keylocking in O (OFF) position

  4. Main contacts position indicator

  5. Spring-charged and ready-to-close indicator

  6. Padlocking in O (OFF) position

  7. Manual/automatic operating mode selector

  8. Closing (I) and opening (O) pushbuttons

  9. Sealing accessory

  10. Trip unit (circuit breaker only)

For more information about motor mechanism installation, consult the instruction sheets on the Schneider Electric website:

NOTE: The motor mechanism cannot be installed on a ComPacT NSX DC EP circuit breaker.

Main Contacts Position Indicator

Indicator

Description

The circuit breaker is closed.

The circuit breaker is open or tripped.

NOTE: Use the SD or SDE switch to distinguish the Trip position from the O (OFF) position.

Control Charge Indicator

Indicator

Description

Stored energy control charged

Stored energy control discharged

NOTE: Stored energy control only provides the necessary energy to close the circuit breaker. The circuit breaker mechanism supplies the energy for tripping.

Manu/Auto Selector

The Manu/Auto button selects the operating mode:

  • In manual operating mode, all electrical commands are disabled.

  • In automatic operating mode, only electrical commands are executed.

NOTE: The opening (O (OFF-T)) pushbutton can be used to open the ComPacT NSX DC circuit breakers in automatic and in manual operating modes.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?