DOCA0186EN-02

BSCM Modbus SL/ULP Module Firmware Update

Introduction

The primary reason for updating the firmware of a BSCM Modbus SL/ULP module is to obtain the latest BSCM Modbus SL/ULP features. If the latest BSCM Modbus SL/ULP features are not required, it is not mandatory to update the firmware of the BSCM Modbus SL/ULP module and the Enerlin’X devices of the IMU.

The BSCM Modbus SL/ULP module remains operational and is able to communicate during firmware update.

For all firmware updates, use the latest version of EcoStruxure Power Commission software.

For more information about firmware updates, refer to DOCA0329EN ComPacT NSX BSCM Modbus SL/ULP Module - Firmware Release Notes.

Checking the Firmware Version

Check the BSCM Modbus SL/ULP module firmware version with EcoStruxure Power Commission software.

After updating the firmware version of the BSCM Modbus SL/ULP module, use the latest version of EcoStruxure Power Commission software to check the firmware compatibility between the IMU devices. The Firmware Update table helps you to diagnose and identify all discrepancy issues between the IMU devices. This table also provides the recommended actions relevant to the detected discrepancies.

Updating Firmware With EcoStruxure Power Commission Software

The prerequisites for updating the firmware with EcoStruxure Power Commission software are the following:

  • Download and install the latest version of EcoStruxure Power Commission software on the PC.

  • Connect the PC to a power supply and deactivate standby mode to avoid the possibility of interruption during the update.

  • In Modbus SL only mode or in Modbus SL and ULP mode, connect the PC to an RJ45 port of the Modbus SL hub.

  • In ULP only mode, connect the PC to the Service Interface or USB maintenance module connected to the RJ45 connector of a ULP module connected to the BSCM Modbus SL/ULP module (for example, IFM Modbus SL communication interface).

The Administrator password of the BSCM Modbus SL/ULP module is required to launch the BSCM Modbus SL/ULP firmware update. For more information, refer to EcoStruxure Power Commission Online Help.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.