DOCA0186EN-02

TM-D Thermal-Magnetic Trip Unit for 3P and 4P Circuit Breakers up to 63 A

Introduction

TM-D thermal-magnetic trip units for 3P/4P circuit breakers up to 63 A are interchangeable trip units.

They are designed for AC and DC general-purpose applications.

The TM-D interchangeable 3P/4P trip units provide:

  • adjustable thermal threshold

  • fixed magnetic pickup

Description

The setting range and adjustment dials are on the front of the trip unit.

A Setting range for TM-D thermal-magnetic 3P/4P trip unit

B Adjustment dial for the thermal protection pickup Ir

Setting the Thermal Protection

The thermal protection pickup Ir is set by a 4-setting dial.

Turning the thermal protection adjustment dial (A) modifies the trip curve as shown (B).

The following table shows the values of the pickup Ir (in amperes) for thermal protection (values indicated on the dial) with respect to every trip unit rating, relative to the position of the dial Ir.

Trip unit rating In (A) at 40 °C (104 °F)

16

25

32

40

50

63

Pickup Ir (A) at 40 °C (104 °F)

11

18

22

28

35

44

13

20

26

32

40

50

14

23

29

36

45

57

16

25

32

40

50

63

Setting the Magnetic Protection

The magnetic protection pickup Ii cannot be adjusted and equals the value shown below:

Trip unit rating In (A)

16

25

32

40

50

63

Fixed pickup Ii (A) +/– 20%

DC value

260

400

550

700

700

700

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.