TM-DC Thermal-Magnetic Trip Unit for 3P and 4P Circuit Breakers from 250 A to 600 A
Introduction
The TM-DC thermal-magnetic trip unit for 3P/4P circuit breakers from 250 A to 600 A are built-in trip units.
They are designed for DC general-purpose applications.
The TM-DC 3P/4P trip units provide:
-
adjustable thermal threshold
-
adjustable magnetic pick-up
Description
Setting the Thermal Protection
The thermal protection pick-up Ir is set by a 5-setting dial.
Turning the thermal protection adjustment dial (A) modifies the trip curve as shown (B).
The following table shows the values of the pick-up Ir (in amperes) for thermal protection (values indicated on the dial) with respect to every trip unit rating, relative to the position of the dial Ir.
|
Trip Unit Rating In (A) at 40 °C (104 °F) |
||||
|---|---|---|---|---|
|
250 |
320 |
400 |
500 |
600 |
|
Pick-up Ir (A) at 40 °C (104 °F) |
||||
|
175 |
224 |
280 |
350 |
420 |
|
200 |
256 |
320 |
400 |
480 |
|
225 |
288 |
360 |
450 |
540 |
|
250 |
320 |
400 |
500 |
600 |
Setting the Magnetic Protection
The magnetic protection pick-up cannot be adjusted and equals the value shown below:
|
Trip Unit Rating In (A) |
||||
|---|---|---|---|---|
|
250 |
320 |
400 |
500 |
600 |
|
Pick-up Ii (A) +/– 20% |
||||
|
625 |
800 |
1000 |
1250 |
1500 |
|
750 |
960 |
1200 |
1500 |
1800 |
|
875 |
1120 |
1400 |
1750 |
2100 |
|
1000 |
1280 |
1600 |
2000 |
2400 |
|
1125 |
1440 |
1800 |
2250 |
2700 |
|
1250 |
1600 |
2000 |
2500 |
3000 |