DOCA0186EN-02

SD Auxiliary Contact for BSCM Modbus SL/ULP Module

Introduction

If the BSCM Modbus SL/ULP module is in Modbus SL only mode, the circuit breaker trip (SD) status is provided to the BSCM Modbus SL/ULP module by using the SD auxiliary contact for BSCM Modbus SL/ULP module.

The commercial reference for the SD auxiliary contact for BSCM Modbus SL/ULP module is LV434210.

Description

The SD auxiliary contact for BSCM Modbus SL/ULP module is optional. When it is connected to the BSCM Modbus SL/ULP module in Modbus SL only mode, it indicates that the circuit breaker has tripped due to:

  • Operation of the MX or MN voltage releases

  • Operation of the push-to-trip button

No.

Data medium

Data transmitted

Comments

A

SD auxiliary contact for BSCM Modbus SL/ULP microswitch

State of SD contact

The SD auxiliary contact for BSCM Modbus SL/ULP module goes into the SD slot instead of the auxiliary contact.

B

Internal link to the BSCM Modbus SL/ULP module

Communication network

With the BSCM Modbus SL/ULP module, the SD auxiliary contact for BSCM Modbus SL/ULP module also transmits the circuit breaker states.

Installation

The slots used to install the SD auxiliary contact for BSCM Modbus SL/ULP module depend on the circuit breaker type.

ComPacT NSX100-250 DC 3P/4P

ComPacT NSX400-630 DC 3P/4P
ComPacT NSX1200 DC 2P

A SD auxiliary contact for BSCM Modbus SL/ULP module

B BSCM Modbus SL/ULP module

The SD auxiliary contact for BSCM Modbus SL/ULP module cannot be installed at the same time as the SD contact.

The SD auxiliary contact for BSCM Modbus SL/ULP module can be installed on site.

For more information about installation, consult the instruction sheet on the Schneider Electric website: GHD16256AA 24 Vdc Terminal Block and SD Auxiliary Contact for BSCM Modbus SL/ULP.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.