DOCA0186EN-02

TM-DC EP Thermal-Magnetic Trip Unit for 4P Circuit Breakers for 1500 Vdc Applications

Introduction

The TM-DC EP thermal-magnetic trip unit for 4P circuit breakers from 100 A to 500 A are built-in trip units.

They are designed for DC photovoltaic and marine applications.

The TM-DC EP 4P trip units provide:

  • adjustable thermal threshold

  • fixed magnetic pick-up on trip units with In from 100 A to 250 A

  • adjustable magnetic pick-up on trip units with In from 250 A to 500 A

Description

The setting range and adjustment dials are on the front of the trip unit.

A Setting range for TM-DC EP thermal-magnetic trip unit

B Adjustment dial for the thermal protection pick-up Ir

C Adjustment dial for the magnetic protection pick-up Ii (on trip units with In from 250 A to 500 A only)

Setting the Thermal Protection

The thermal protection pick-up Ir is set by a 4-setting dial.

Turning the thermal protection adjustment dial (A) modifies the trip curve as shown (B).

The following table shows the values of the pick-up Ir (in amperes) for thermal protection (values indicated on the dial) with respect to every trip unit rating, relative to the position of the dial Ir.

Trip Unit Rating In (A) at 50 °C (122 °F)

250 A frame 500 A frame

100

125

160

200

250

250

320

400

500

Pick-up Ir (A) at 50 °C (122 °F)

70

87

112

140

175

175

224

280

350

80

100

128

160

200

200

256

320

400

90

112

144

180

225

225

288

360

450

100

125

160

200

250

250

320

400

500

The thermal protection setting is fixed at the trip unit rating.

Setting the Magnetic Protection on Trip Units With In from 100 A to 250 A

For trip units rated below 250 A, the magnetic protection pick-up cannot be adjusted and equals the value shown below:

 

Trip Unit Rating In (A)

100

125

160

200

250

Fixed Pick-up Ii (A) +/– 20%

DC value

600

750

960

1,200

1,500

Setting the Magnetic Protection on Trip Units With In from 250 A to 500 A

For trip units rated between 250 A and 500 A, the magnetic protection pick-up Ii is set by a 6-setting dial.

Turning the magnetic protection adjustment dial (A) modifies the trip curve as shown (B).

The following table shows the values of the pick-up Ii (in amperes) for magnetic protection (values indicated on the dial), relative to the position of the Ii dial:

Trip Unit Rating In (A)

250

320

400

500

Pick-up Ii (A) +/– 20%

1,250

1,600

2,000

2,500

1,500

1,920

2,400

3,000

1,750

2,240

2,800

3,500

2,000

2,560

3,200

4,000

2,250

2,880

3,600

4,500

2,500

3,200

4,000

5,000

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.