DOCA0185EN-01

Insulation Accessories

Overview of Insulation Accessories

The following insulation accessories can be used with the range of ComPacT NSXm circuit breakers. For more information, see LVPED217032EN ComPacT NSX & NSXm Catalogue.

Insulation accessory

All power connectors

3P

4P

Long terminal shield

Interphase barriers

Rear insulation screen

Presentation of Insulation Accessories

The following insulation accessories can be installed on-site.

Insulation accessory

Benefit

Accessory image

Long terminal shield

IP40 protection

Flexible interphase barriers

Improve insulation between power connections

Rear insulation screen

Improve insulation between backplate and power connections, especially with spreaders

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.