DOCA0185EN-01

SDx Module

Introduction

One or two optional SDx modules can be installed on an earth-leakage circuit breaker (ELCB).

The SDx module has two outputs and provides alarms and fault differentiation.

The SDx module receives data from the trip unit through an optical link.

Description

A Power supply

B Output 2 (1NO+1NC)

C Output 1 (1NO+1NC)

D Lock knob

E SDx module status

  • OFF: SDx module not powered

  • Green: SDx module powered

F Output 1 setting dial

G Output 1 status LED

  • OFF: output de-activated

  • Red: output activated

H Output 2 setting dial

I Output 2 status LED

  • OFF: output de-activated

  • Red: output activated

J Seal for setting cover

K Clips to attach to ELCB

SDx Module Characteristics

Power supply: 24–240 Vac/Vdc

Power:

  • 2,000 VA maximum

  • 240 W maximum

Output characteristics:

  • Voltage: 24–250 Vac/Vdc

  • Current: 2 mA–5 A maximum

Output Settings

The function assigned to each output of the SDx module is set by using a setting dial. Each output can be assigned with one of the following indications:

  • Overload trip indication (SDT): circuit breaker has tripped due to an overload fault.

  • Overload alarm (SDT105%): current is higher than 105% of the setting current (Ir).

  • Earth-leakage alarm (SDV80%): leakage current is higher than 80% of the earth-leakage trip threshold (IΔn).

  • Earth-leakage trip indication (SDV): circuit has tripped due to an earth-leakage current.

T

SDT thermal fault indication

T105%

SDT thermal alarm: 105% Ir

V80%

SDV earth-leakage alarm: 80% IΔn

V

SDV earth-leakage fault indication

SDT and SDT105% Operating Modes

Operating modes of the SDT output:

  • The output is activated when the circuit breaker trips due to an overload fault.

  • The output is reset when the circuit breaker is reset, closed, and energized.

Operating modes of the SDT105% output:

  • The output is activated when current is greater than 105% x Ir.

  • The output is reset in one of the following cases:

    • The current is lower than 105% x Ir.

    • After tripping, the circuit breaker is reset, closed, and energized.

I

Charge current

SDT105%

Thermal alarm

SDT

Thermal fault indication

Q

Circuit breaker

SDV and SDV80% Operating Modes

Operating modes of the SDV output:

  • The output is activated when the circuit breaker trips due to an earth-leakage fault.

  • The output is reset when the circuit breaker is reset, closed, and energized.

Operating modes of the SDV80% output:

  • The output is activated when the earth-leakage current is greater than 80% x IΔn for more than 5 seconds.

  • The output is reset in one of the following cases:

    • The current is lower than 80% x IΔn.

    • After tripping, the circuit breaker is reset, closed, and energized.

IΔn

Earth-leakage current

SDV80%

Earth-leakage alarm

SDV

Earth-leakage fault indication

Q

Circuit breaker

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.