DOCA0185EN-01

Description

Front Face

The controls, indicators, and locking mechanism are located on the following parts of the circuit breaker:

  • The operating control is on the side plate.

  • The operation indicators are on the circuit breaker and on the side plate.

  • The locking mechanism is on the side plate.

The following figure shows the controls and indicators for a circuit breaker with a side rotary handle. Information about the other parts of the front face is available in the general description.

A Side rotary handle

B Device identification

C QR code

D Push-to-trip button

For more information about installation, consult the instruction sheet on the Schneider Electric website: NNZ4765107 Side Rotary Handle - Instruction Sheet

Device Identification

Information about the circuit breaker is given on the device identification label.

QR Code

Scan the QR code to get additional information about the circuit breaker from the Schneider Electric website. To scan the QR code, use a smartphone that is equipped with a camera and installed with a QR code reader.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.