DOCA0185EN-01

Locking the Circuit Breaker

Locking Options for the Toggle Handle

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
When the circuit breaker handle is locked in the (O) OFF position, always use a properly rated voltage sensing device to confirm that power is off before working on equipment.
Failure to follow these instructions will result in death or serious injury.
NOTE: Locking the handle in the I (ON) position does not disable the circuit breaker. If an electrical fault is detected, the circuit breaker trips. When the handle is unlocked, it moves to the (Trip) position. To return the circuit breaker to service, reset the circuit breaker.

The following accessories can be used to lock the toggle handle:

Locked position Lock type Lock characteristics Lock image

O (OFF)

Fixed: the device cannot be removed from the case.

Up to 3 padlocks (not supplied)
Diameter 4–8 mm (3/16–5/16 in.)

O (OFF)

Removable: the device can be removed from the case.

Up to 3 padlocks (not supplied)
Diameter 4–8 mm (3/16–5/16 in.)

I (ON) or O (OFF)

Fixed: the device cannot be removed from the case.

Up to 3 padlocks (not supplied)
Diameter 4–8 mm (3/16–5/16 in.)

Locked in the I (ON) position.

Locked in the O (OFF) position.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.