DOCA0185EN-01

Feature Overview

Feature Overview

ComPacT NSXm devices have the following features:

  • Circuit breakers rated from 16 to 160 A

  • Available constructions: 3 and 4 poles

  • Standard compliance to IEC/EN 60947-2 (circuit breakers and earth-leakage circuit breakers) and IEC/EN 60947-3 (switch-disconnectors)

  • Breaking capacities: 16, 25, 36, 50, 70 kA at 415 Vac

  • Voltage up to 440 Vac for earth-leakage circuit breakers (compliance to IEC/EN 60947-2)

  • Voltage up to 690 Vac for circuit breakers (compliance to IEC/EN 60947-2) and switch-disconnectors (compliance to IEC/EN 60947-3)

  • Field installable electrical accessories

  • Optional terminations

  • Optional operating mechanisms

  • Optional voltage releases

  • Optional auxiliary contacts

  • Optional insulation accessories

  • Optional locking accessories

Isolation Characteristics

Circuit breakers offer positive contact indication and are suitable for isolation in accordance with standards IEC/EN 60947-2 and IEC/EN 60947-3.

The following markings on the device identification label indicate that the devices are capable of isolation:

Circuit breaker
Switch-disconnector

To confirm the isolation capability, the IEC/EN 60947-2 and 3 standards require specific shock withstand tests.

In accordance with installation rules, circuit breakers can be locked in the O (OFF) position so that work can be carried out with the power off. Circuit breakers can be locked in the O (OFF) position only when they are open.

NOTE: Locking a circuit breaker in the O (OFF) position is sufficient to isolate the circuit breaker.

The choice of locking device depends on the type of actuator:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.