DOCA0185EN-01

Device Overview

Circuit Breaker and Switch-Disconnector Description

A Power connection (EverLink lug, EverLink lug with control wire terminal, compression lug / busbar, mechanical lug)

B Connection system cover

C QR code to product information

D Toggle handle

E Window showing LED on electrical auxiliary device installed on device, for example SD auxiliary contact

F Device identification, certification marks, and IEC/EN interrupting ratings

G Product and accessory data labels

H Push-to-trip button

I Seal for setting cover

J Tripping curve

K DIN rail lock

L Current setting button (for circuit breaker only)

M Window showing LED on electrical auxiliary device installed on device, for example OF auxiliary contact

N MN or MX presence indicator

O Seal for accessory cover

Earth-Leakage Circuit Breaker (ELCB) Description

A Power connection (EverLink lug, EverLink lug with control wire terminal, compression lug / busbar, mechanical lug)

B Connection system cover

C QR code to product information

D Toggle handle

E Window showing LED on electrical auxiliary device installed on device, for example SD auxiliary contact

F Product and accessory data labels

G Device identification, certification marks, and IEC/EN interrupting ratings

H Push-to-trip button

I Seal for setting cover

J Trip unit

K Switch to isolate the device during dielectric tests

L DIN rail lock

M Current rating and protection setting range

N Test button of earth-leakage protection

O Earth-leakage trip indication

P Window showing LED on electrical auxiliary device installed on device, for example OF auxiliary contact

Q MN or MX presence indicator

R Seal for accessory cover

The trip unit is described in a specific topic.

QR Code

Scan the QR code to get additional information about the circuit breaker from the Schneider Electric web site. To scan the QR code, use a smartphone that is equipped with a camera and installed with a QR code reader.

Accessories

The following accessories are available for the circuit breaker.

A Compression lug / busbar connector

B EverLink lug without control wire terminal

C Aluminum mechanical lug

D EverLink lug with control wire terminal

E Torque limiting breakaway bits

F Long terminal shield

G Interphase barriers

H Rear insulating screen

I MN or MX voltage release

J MN undervoltage release pre-wired

K MX shunt trip pre-wired

L OF or SD auxiliary contact

M OF auxiliary contact pre-wired

N SD auxiliary contact pre-wired

O Wireless indication auxiliary

P Side rotary handle (right or left)

Q Extended rotary handle

R Open door shaft operator

S Direct mounted rotary handle

T SDx module (for earth-leakage circuit breaker only)

U PowerTag Energy F160

V Removable toggle handle padlocking device (OFF only)

W Fixed toggle handle padlocking device (OFF and ON)

X Fixed toggle handle padlocking device (OFF only)

Y Terminal spreaders

Sealing Accessories

The following sealing accessories can help prevent unauthorized changes to the circuit breaker.

Seal type

Helps to prevent

Seal image for circuit breaker

Seal image for earth-leakage circuit breaker

Seal for cover

  • Removal of the front cover

  • Access to the auxiliaries

Seal for long terminal shield

  • Access to the power connections (helps to prevent direct contact)

  • Dismounting of the circuit breaker

Seal for settings

  • Access to settings

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.