PowerTag Energy F160
Introduction
The PowerTag Energy F160 is suitable for molded case circuit breakers and switch-disconnectors (ComPacT NSXm and ComPact INS) for 3P and 3P+N electrical networks.
The PowerTag Energy F160 is mounted above or below the circuit breaker using conductor feedthroughs for current measurement. .
With its Flex design, the PowerTag Energy F160 is mounted directly on the power cables. Voltage take-off must be wired, using the recommended EverLink connectors with control wire terminal (LV426970 for 3P, LV426971 for 4P).
The PowerTag Energy F160 must be associated with a concentrator or gateway.
For more information about installation, consult the instruction sheet on the Schneider Electric website: MFR85580 PowerTag F160 3P/3P+N – Instruction Sheet
Description
Status LED
Data Available
To get the list of data available, refer to the relevant gateway or Panel Server user guide. Data available depends on the gateway.
Commissioning
Commission the PowerTag Energy F160 by using EcoStruxure Power Commission software or the embedded webpages of the gateway or panel server, if any.
For automatic pairing the PowerTag Energy F160 must be powered and the Status LED must be flashing fast orange.
If the LED is flashing fast red (loss of communication status), turn the power off and on to reset the PowerTag Energy F160. If the PowerTag Energy F160 is not paired within two minutes, it returns to loss of communication status.
If the LED is blinking green, PowerTag Energy F160 is already paired with a gateway. Unpair it before pairing with a new gateway.