990-6392E-001

Connect the Power Cables for 3:1 Systems

  1. Connect the PE cable.
  2. Perform one of the following:
    • For single mains: Connect the input cables.
    • For dual mains: Connect the bypass cables.
  3. Connect the UPS output cables.
  4. Connect the load cables.
  5. Fasten the cables with cable ties to the cable reliefs.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?