990-6392E-001

Overview of Easy UPS 3-Phase Modular System with Maintenance Bypass Panel

UIB Unit input breaker
SSIB Static switch input breaker
UOB Unit output switch
IMB Internal maintenance switch
MBB Maintenance bypass switch
BB Battery breaker

Easy UPS 3-Phase Modular Parallel System

Parallel System – Single Mains (One Internal Switch)

Parallel System – Dual Mains (One Internal Switch)

Parallel System – Single Mains (Four Internal Switches)

Parallel System – Dual Mains (Four Internal Switches)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?