990-6392E-001

Overview of Easy UPS 3M Advanced System with Maintenance Bypass Panel

UIB Unit input breaker
SSIB Static switch input breaker
UOB Unit output switch
IMB Internal maintenance switch
MBB Maintenance bypass switch
BB Battery breaker

Easy UPS 3M Advanced Single System – Single Mains

Easy UPS 3M Advanced Single System – Dual Mains

Easy UPS 3M Advanced Parallel System

Parallel System – Single Mains

Parallel System – Dual Mains

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.