Important Safety Instructions — SAVE THESE INSTRUCTIONS
Read these instructions carefully and look at the equipment to become familiar with it before trying to install, operate, service or maintain it. The following safety messages may appear throughout this manual or on the equipment to warn of potential hazards or to call attention to information that clarifies or simplifies a procedure.
![]() |
---|
DANGER indicates a hazardous situation which, if not avoided, will result in death or serious injury.
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
WARNING indicates a hazardous situation which, if not avoided, could result in death or serious injury.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
![]() |
---|
CAUTION indicates a hazardous situation which, if not avoided, could result in minor or moderate injury.
Failure to follow these instructions can result in injury or equipment damage.
|
NOTICE |
---|
NOTICE is used to address practices not related to physical injury. The safety alert symbol
shall not be used with this type of safety message.
Failure to follow these instructions can result in equipment damage.
|
Please Note
Electrical equipment should only be installed, operated, serviced, and maintained by qualified personnel. No responsibility is assumed by Schneider Electric for any consequences arising out of the use of this material.
A qualified person is one who has skills and knowledge related to the construction, installation, and operation of electrical equipment and has received safety training to recognize and avoid the hazards involved.
Electromagnetic Compatibility
NOTICE |
---|
Risk of electromagnetic disturbance
This is a product Category C3 according to IEC 62040-2. This is a product for commercial
and industrial applications in the second environment - installation restrictions
or additional measures may be needed to prevent disturbances. The second environment
includes all commercial, light industry, and industrial locations other than residential,
commercial, and light industrial premises directly connected without intermediate
transformer to a public low-voltage mains supply. The installation and cabling must
follow the electromagnetic compatibility rules, e.g.:
Failure to follow these instructions can result in equipment damage.
|
Safety Precautions
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
All safety instructions in this document must be read, understood and followed.
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Read all instructions in the Installation Manual before installing or working on this
UPS system.
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
hazard of electric shock, explosion, or arc flash
Do not install the UPS system until all construction work has been completed and the
installation room has been cleaned.
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
The UPS system must be installed according to local and national regulations. Install
the UPS according to:
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
hazard of electric shock, explosion, or arc flash
The UPS is not designed for and must therefore not be installed in the following unusual
operating environments:
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
Hazard of electric shock, explosion, or arc flash
Do not drill or cut holes for cables or conduits with the gland plates installed and
do not drill or cut holes in close proximity to the UPS.
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
HAZARD OF ARC FLASH
Do not make mechanical changes to the product (including removal of cabinet parts
or drilling/cutting of holes) that are not described in the Installation Manual.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
NOTICE |
---|
risk of overheating
Respect the space requirements around the UPS system and do not cover the product’s
ventilation openings when the UPS system is in operation.
Failure to follow these instructions can result in equipment damage.
|
NOTICE |
---|
risk of equipment damage
Do not connect the UPS output to regenerative load systems including photovoltaic
systems and speed drives.
Failure to follow these instructions can result in equipment damage.
|
Electrical Safety
![]() |
---|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
Hazard of electric shock, explosion, or arc flash
In systems where backfeed protection is not part of the standard design, an automatic
isolation device (backfeed protection option or other device meeting the requirements
of IEC/EN 62040–1 or UL1778 5th Edition – depending on which of the two standards apply to your local
area) must be installed to prevent hazardous voltage or energy at the input terminals
of the isolation device. The device must open within 15 seconds after the upstream
power supply fails and must be rated according to the specifications.
Failure to follow these instructions will result in death or serious injury.
|
When the UPS input is connected through external isolators that, when opened, isolate the neutral or when the automatic backfeed isolation is provided external to the equipment or is connected to an IT power distribution system, a label must be fitted at the UPS input terminals, and on all primary power isolators installed remote from the UPS area and on external access points between such isolators and the UPS, by the user, displaying the following text (or equivalent in a language which is acceptable in the country in which the UPS system is installed):
![]() |
---|
Hazard of electric shock, explosion, or arc flash
Risk of Voltage Backfeed. Before working on this circuit: Isolate the UPS and check
for hazardous voltage between all terminals including the protective earth.
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
Risk of electrical disturbance
This product can cause a DC current in the PE conductor. Where a residual current-operated
protective device (RCD) is used for protection against electrical shock, only an RCD
of Type B is allowed on the supply side of this product.
Failure to follow these instructions can result in injury or equipment damage.
|
Battery Safety
![]() |
---|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
Hazard of electric shock, explosion, or arc flash
Batteries can present a risk of electric shock and high short-circuit current. The
following precautions must be observed when working on batteries
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
Hazard of electric shock, explosion, or arc flash
When replacing batteries, always replace with the same type and number of batteries
or battery packs.
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
risk of equipment damage
Failure to follow these instructions can result in injury or equipment damage.
|