990-6289H-001

Input Power Factor

The values are at a 400 V 50 Hz linear load.

UPS rating 250 kVA 300 kVA 400 kVA 500 kVA 600 kVA
25% load 0.99 0.99 0.99 0.98 0.98
50% load 0.99 0.99 0.99 0.99 0.99
75% load 0.99 0.99 0.99 0.99 0.99
100% load 0.99 0.99 0.99 0.99 0.99
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.