990-6289H-001

End of Discharge Voltage

The Low Battery Shutdown level is 1.6 V per cell depending on discharge ratio.

The Low Battery Shutdown level is 1.61 V to 1.74 V per cell depending on discharge ratio.

The Low Battery Shutdown level is 1.75 V per cell depending on discharge ratio.

The Low Battery Shutdown level is 1.76 V to 1.8 V per cell depending on discharge ratio.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.