990-6204D-001

Communication Interfaces

  1. Parallel ports

  2. CAN_R: CAN termination resistor

  3. Dry contacts

  4. USB port

  5. EPO

  6. Slot for optional cold start button

  7. Network management card (NMC)

  8. Load bus synchronization port

  9. RS485

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.