990-6204D-001

Install Batteries in the UPS

DANGER
hazard of electric shock, explosion, or arc flash
Ensure that the battery breakers (BB) are in the off position before installing batteries.
Failure to follow these instructions will result in death or serious injury.
  1. Remove the plate in front of the battery shelves.
  2. Install battery modules one string at a time and from the bottom and up. One row is one battery string.
  3. Fasten the battery modules with a screw in front of the battery module
  4. Remove the shrink tubes from the power terminals and connect the power terminals to the batteries.
  5. Reinstall the plate in front of the battery shelves.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.