990-6204D-001

Route the Signal Cables

  1. Remove the indicated plate from the front of the UPS.
  2. Remove the rear gland plate and the rear brush plate from the UPS.
    1. For installations without conduits, reinstall the brush plate.

    2. For installations with conduits, drill holes for conduits and reinstall the gland plate.

  3. Route the signal cables through the gland/brush plate and to the front of the UPS.
  4. Reinstall the plate on the front of the UPS.
  5. Fasten the signal cables with cable ties on the rear of the UPS.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.