990-6204D-001

Connect the Power Cables

  1. Ensure that all breakers are in the OFF (open) position.
  2. Remove the two bottom rear panels.

    Rear View of the UPS

  3. Remove the indicated plate.
  4. In dual mains systems, remove the three single mains brackets.
  5. In TNC systems only, rotate the jumper busbar to create a connection between the PE busbar and the neutral busbar.
  6. Route the power cables through the bottom of the UPS.
  7. Connect the PE cable to the PE terminal.

    Single Mains System

    Dual Mains System

  8. Connect the input, output, and bypass (if applicable) cables.
  9. For installation with modular battery cabinets, connect the battery cables:
    1. Remove the indicated cover.
    2. Connect the battery cables.
    3. Reinstall the cover over the battery terminals.
  10. Fasten the cables to the cable relief in the bottom of the UPS.
  11. Reinstall the plate and the rear panels.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.