990-66230B-001

View the Battery Solution Configuration

  1. From the main menu, tap Configuration > Battery.
  2. View the battery settings on the display. Tap the arrow symbol to go to the next page.
    NOTE: The battery settings are only configurable by a Schneider Electric Services Representative.
    Battery type Shows the battery type: VRLA.
    Battery number Shows the number of battery cells. The battery number can be set to 32, 34, 36, 38, or 40, default is 40.
    Battery capacity Shows the total battery capacity (string quantity x Ah/string), default is 20 Ah.
    Float charge voltage/cell Shows the float voltage per battery cell.
    Float charging is the basic charging function available on all types of batteries and automatically initiated by the charger. The range for float charge voltage/cell is 2.10-2.35 V, default is 2.25 V.
    Boost charge voltage/cell Shows the boost voltage per battery cell.

    Boost charging makes it possible to conduct a fast charging in order to quickly restore a discharged battery. The range for boost charge voltage/cell is 2.20 - 2.45 V, default is 2.25 V.

    Charge current percent limit Shows the maximum percentage of the charging current. The range for charge current percent limit varies*, default is 10%.
    Charge current limitation by Ah Shows the charge current limitation according to the Ah ratio. The limited current can be set to 0.10 C, 0.15 C, 0.20 C, or 0.25 C, default is 0.25 C.
    Charge sleep time Shows the sleep time for charging. The range for the charge sleep time is 3 - 14400 minutes, default is 3 minutes. When the battery reaches the target voltage, charging will automatically stop based on the pre-set charge sleep time.
    EOD voltage/cell at 3C current Shows the EOD voltage per battery cell for 3C current. The range for EOD voltage/cell at 3C current is 1.6-1.85 V, default is 1.65 V.
    EOD voltage/cell at 0.05C current Shows the EOD voltage per battery cell for 0.05C current. The range for EOD voltage/cell at 0.05C current is 1.65-1.90 V, default is 1.75 V.
    Allow boost charge Shows if boost charge is allowed. Boost charging makes it possible to conduct a fast charging in order to quickly restore a discharged battery. The default setting is Disable.
  3. Tap OK to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?