990-66230B-001

Configure the Rating

NOTE: This configuration is mandatory for correct UPS operation.
  1. From the main menu, tap Configuration > Rating.
    1. Set Rated output voltage to 220 V, 230 V, or 240 V, default is 230 V.
    2. Set Rated output frequency to 50 Hz or 60 Hz , default is 50 Hz.
    NOTE: The Rated power is not configurable.
  2. Tap OK to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?