990-66230B-001

Overview of User Interface

Display

Overview of the Home Screen

  1. Home button - tap here on any screen to return to the home screen.

  2. Main menu button - tap here to access the menus.

  3. Mimic diagram button - tap here to access the mimic diagram.

  4. Alarm status symbol - tap here to access the active alarms log.

  5. Commercial reference - shows the product commercial reference.

  6. Parallel information - shows the parallel information for a parallel system when System mode is set to Parallel. The first digit represents the parallel number in a system while the second digit indicates the parallel ID of the current UPS.

You can tap on the input, output, or battery fields on the home screen to go directly to the detailed measurement pages.

Main Menu


Tap the main menu button on the home screen to access the menus.

Mimic Diagram

Tap the mimic diagram button on the home screen to access the mimic diagram.

The mimic diagram will adapt to your system configuration – the mimic diagram shown here is just an example.

Example of Single UPS System – Single Mains

The green power line (gray in illustration) in the mimic diagram shows the power flow through the UPS system. Active modules (inverter, rectifier, battery, static bypass switch, etc.) are framed in green and inactive modules are framed in black. Modules framed in red are inoperable or in an alarm condition.

In mimic diagrams for parallel systems, tap on the gray UPS to see the mimic diagram on UPS level. The numbers after UPS 0-3 represent the individual Parallel ID for the UPS.

Example of Parallel System

Menu Tree


Tap the main menu button on the home screen to access the menus.

  • Status

    • Input

    • Output

    • Bypass

    • Battery

    • Temperature

  • Logs

  • Control*

    • Operation mode

    • Inverter

    • Charger

  • Configuration*

    • UPS

    • Input

    • Output

    • Bypass

    • Rating

    • Battery

    • Communication

    • Contacts and relays

    • Reminders

    • General

    • Network

  • Maintenance*

    • Buzzer

    • Battery

    • S-code

    • Alarm clear

    • UPS report

  • About

  • Logout

  • Digital experience

  • Language

Some menus contain more submenus than described in this manual. These submenus are grayed out and are only for use by Schneider Electric to avoid unwanted load impacts. Other menu items can also be grayed out/not shown on the display if they are not relevant or not released yet for this particular UPS system.

Alarm Status Symbols

The alarm status symbol (gray in illustration) in the top right corner of the display changes depending on the alarm status of the UPS system.

Green: No alarms present in the UPS system.
Blue: Informational alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log.
Yellow: Warning alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log.
Red: Critical alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log.
Red: Connection from the display to the UPS is lost.

Location of Disconnect Devices

Rear View of 10-20 kVA UPS (Internal Batteries)

Rear View of 30-40 kVA UPS (Internal Batteries)

Rear View of 10-20 kVA UPS (External Batteries)



Rear View of 30-40 kVA UPS (External Batteries)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?