990-66230B-001

Turn the Inverter ON

NOTE: This function is only available if enabled by Service.
  1. From the main menu, tap Control > Inverter > Inverter on.
  2. Tap OK on the confirmation screen.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?