990-66230B-001

Configure the UPS

NOTE: This configuration is mandatory for correct UPS operation.
  1. From the main menu, tap Configuration > UPS.
    1. Set System mode to Single, Parallel, Single ECO, Parallel ECO or Self-aging, default is Single.
    2. Set Parallel number to 1, 2, 3, or 4, default is 1.
    3. Set Parallel ID to 0, 1, 2, or 3, default is 0.
    4. Set Slew rate to 0.5 Hz/s, 1.0 Hz/s, 1.5 Hz/s, or 2.0 Hz/s, default is 2.0 Hz/s.
    5. Set System autostart mode after EOD to Normal, Only bypass, or No output, default is Normal. When System autostart mode after EOD has been enabled, the inverter will start up automatically when input voltage returns, after a shutdown due to drained battery.
      WARNING
      Hazard of electric shock, explosion, or arc flash
      Always perform correct Lockout/Tagout before working on the UPS. A UPS with autostart enabled will automatically restart when the mains supply returns.
      Failure to follow these instructions can result in death, serious injury, or equipment damage.
  2. Tap OK to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?