990-66230B-001

Find the Serial Numbers

  1. From the main menu, tap About.
  2. Note down the serial number of the UPS cabinet and have it ready for customer support.
    NOTE: If the display is not available, look at the top of the UPS and find the UPS serial number on the name plate label under SERIAL:

    Example of Name Plate Label for UPS

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?