990-66230B-001

View the System Status Information

  1. From the main menu, tap Status.
    1. Tap Input to see the status.

      Input

      Voltage ph-ph (phase-to-phase) The present phase-to-phase input voltage.
      Voltage ph-N (phase-to-neutral)* The present phase-to-neutral input voltage in volts (V).
      Current The present input current from the AC utility power source per phase in amperes (A).
      Frequency The present input frequency in hertz (Hz).
      Power factor The ratio of the active power to apparent power.
    2. Tap Output to see the status.

      Output

      Voltage ph-ph (phase-to-phase) The phase-to-phase output voltage at the inverter in volts (V).
      Voltage ph-N (phase-to-neutral)* The phase-to-neutral output voltage at the inverter in volts (V).
      Current The present output current for each phase in amperes (A).
      Frequency The present output frequency in hertz (Hz).
      Power factor The present output power factor for each phase. Power factor is the ratio of active power to apparent power.
      Power The present active power (or real power) output for each phase in kilowatts (kW). Active power is the portion of power flow that, averaged over a complete cycle of the AC waveform, results in net transfer of energy in one direction.
      Load The percentage of the UPS capacity presently used across all phases. The load percentage for the highest phase load is displayed.
    3. Tap Bypass to see the status.

      Bypass

      Voltage ph-ph (phase-to-phase) The present phase-to-phase bypass voltage (V).
      Voltage ph-N (phase-to-neutral)* The present phase-to-neutral bypass voltage (V).
      Current The present bypass current for each phase, in amperes (A).
      Frequency The present bypass frequency in hertz (Hz).
      Power factor The present bypass power factor for each phase. Power factor is the ratio of active power to apparent power.
    4. Tap Battery to see the status.

      Battery

      Measurements The present DC power being drawn from the battery, in kilowatts (kW).
      The present battery voltage (VDC).
      The present battery current in amperes (A). A positive current indicates that the battery is charging; a negative current indicates that the battery is discharging.
      Battery temperature from the connected temperature sensors in Celsius.
      The status of the battery (Disconnect or Connect).
      Battery The amount of time before the batteries reach the low-voltage shutdown level. Also shows charge level of the battery as a percentage of full charge capacity.
      The present battery charge (Ah).
      Charger The operation mode of the charger (Resting, Float charge, Boost charge, Discharge).
    5. Tap Temperature to see the status.

      Temperature

      Ambient temperature Ambient temperature in Celsius.
      Battery temperature Battery temperature in Celsius from the connected battery temperature sensors.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?