DOCA0343EN-00

Provisioning the Gateway

Perform the following steps to provision the gateway:

  1. Power on the gateway by connecting it to the power source using the power cable provided inside the box.

  2. Wait for the top LED of the gateway to blink red and green alternatively, this should take up to five minutes.

    NOTE: The inserted SIM will be able to get the gateway online automatically. The option to choose between WiFi or Ethernet is available in the later stages.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?