Troubleshooting
The troubleshooting steps for some known issues are listed below:
-
Issue: If the hardware is missing in the box?
-
If you find that essential hardware components are missing from the box, please contact your coordinator for assistance in resolving the hardware mismatch issue.
-
-
Issue: Internet is not working even if an active SIM is installed inside the Flex-Server?
-
If you are experiencing issues with the internet not working, even with an active SIM card installed in the Flex-Server, consider the following steps to resolve the problem:
-
Antenna connection check:
-
Make sure that the antenna is correctly connected, referring to the provided image.
-
If the connection is loose or removed, secure it properly.
-
After resolving the connection issue, wait for 5 minutes for the Flex-Server to come online.
-
-
-
Location or SIM operator change:
-
If the antenna connection is secure and the issue persists, consider changing the location of the Flex-Server.
-
Alternatively, try using a different SIM operator, as the network coverage at the current location may be insufficient.
-
If the problem persists after trying these steps, please contact Schneider Electric for further assistance www.se.com/buildings.

-
-
-
Issue: Flex-Server is on cellular network, however, not coming online.
-
Follow the below steps to get the Flex-Server online:
-
Check the antennas and antenna cables properly connected.
-
Try removing the SIM card and inserting it again.
NOTE: Pin enabled SIM card is not supported.
-
-
-
Issue: Flex-Server is online; however, the data is lost, or delayed response is observed?
-
In case of cellular network:
-
Check the cellular network signal strength on the plotter.
-
Check if the data plan is active on the SIM card.
-
-
In case of Wi-Fi network:
-
Check the Wi-Fi signal strength and speed on the Wi-Fi network using another device (which can be a mobile or a laptop).
-
-
-
Issue: If RS485 port is not sending the data?
-
Follow the below steps if the RS485 port is not sending the data:
-
Check if the connections are done as per the installation instructions.
-
Check if correct port is configured.
-
Check again, if the connections are not reversed.
-
Check for loose wires.
-
Check the Modbus/BACnet ID is correct.
-
Check the baud rate configured for the end device.
-
Check if any loose strand is shorting on the bus or to the ground.
-
Check if any Modbus device is connected to BACnet bus or vice-versa.
-
Check if the number of devices in the loop are as per the specifications in installation instructions.
-
Check if the loading of devices causes the resistance to drop or to increase significantly. You should not connect more than two resistors on a single bus.
-
Check if wires are used as per the specifications in the installation instructions.
-
-
-
Issue: Cannot Edit Compute Module and Carrier Board Number After Commissioning the Flex-Server
-
The Compute Module and Carrier Board Number are unique identifiers. Once mapped to a server, they cannot be edited or reassigned to another server.
-
-
Issue: Network Configuration is Not Visible
-
The network configuration is retrieved directly from the Flex-Server.
-
If the information is missing, it indicates that the Flex-Server is offline, or the dashboard is unresponsive.
-
-
Issue: Next button is always enabled
-
The Next button is designed to navigate to the next page without validating whether changes were saved.
-
If you edit data but does not save it before clicking Next the changes will be lost.
-
-
Issue: Unable to delete Space Configuration
-
Currently, delete functionality is available for equipment only. Space Configuration cannot be deleted at this time.
-
-
Issue: Unable to update Site Card Information
-
The site name, location, and latitude/longitude are defined in the backend and cannot be changed through the dashboard.
-