Site Commissioning Information
Once the gateway is provisioned and is online, the field engineers start installing the other hardware and once all the devices are installed, fill up the below template and share that with the commissioning engineer.
Sl. No. |
Details |
Remarks |
|
1 |
Gateway Details |
Carrier board (Compute Module): [Provide carrier board details] |
|
Compute Module SN: [Provide Compute Module SN] |
|||
Detail Sticker on Gateway Enclosure: [Attach photo or provide details] |
|||
2 |
Site Location |
Latitude: [Provide latitude] |
|
Longitude: [Provide longitude] |
|||
Address: [Provide full address] |
|||
3 |
Hardware Documentation |
Site Name: [Provide Site Name] |
|
Invoice or Delivery Challan: [Attach document or provide details] |
|||
4 |
SIM Details |
SIM Number: [Provide SIM number] |
|
Network Provider: [Provide network provider] |
|||
5 |
Load Mapping Details: |
||
a. Device Information |
Device ID: [Provide Device ID] |
||
Make and Model of Device: [Provide details] |
|||
Number of Assets and their Types: [Specify details] |
|||
Customer Load Details: [Specify details] |
|||
b. Configuration of the Device |
Device Associated with which Asset: [Specify details] |
||
c. Location of the Installed Device |
Device Installation Location: [Specify details] |
||
6 |
Testing Details: |
||
a. Device Connection Check |
Multimeter Reading: [Provide readings] |
For Meter Ampere Matching |
|
b. Asset Control Verification |
Asset Control Status: [Specify status] |
||
7 |
Installed Device Pictures |
[Attach photos of the installed devices] |
|
8 |
Installation Report and Sign-off |
[Attach Installation Report and Sign-off document] |