Assembling the Flex-Server
Refer to the below table for physical description and dimensions:
|
Description |
Image |
|
Mounting bracket for Flex-Server |
|
|
Mounting bracket for LoRa and RS485 |
|
|
Flex-Server dimensions |
|
|
Flex-Server |
|
|
Wi-Fi antenna |
|
|
4G antenna |
|
|
Power supply |
|
|
LoRa Connector |
|
|
RS485 Converter |
Perform the following steps to install the Flex-Server on mounting bracket with power supply:
-
Mark the positions of two drilling holes on the surface to install the mounting bracket.
-
Drill two holes using a drill bit of 6 mm diameter.
-
Install the mounting bracket on the surface with two M4 x 25 mm self-tapping screws.
-
Tighten the screws using PH1 screwdriver.
-
Slide the Flex-Server on the mounting bracket.
DANGERHAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH- Turn off all power supplying this equipment before working on or inside equipment.
Failure to follow these instructions will result in death or serious injury. -
Do the necessary wiring. Refer to the EcoStruxure™ Flex-Server Installation Sheet - ZEN0000102.
NOTE: Use 0.2 A fuse with appropriate line to main voltage between AC power supply and mains.
Perform the following steps to install the LoRa connector and RS485I on mounting bracket:
-
Mark the positions of two drilling holes on the surface to install the mounting bracket.
-
Drill two holes using a drill bit of 6 mm diameter.
-
Install the mounting bracket on the surface with two M4 x 25 mm self-tapping screws.
-
Tighten the screws using PH1 screwdriver.
-
Install two M3 x 6 mm flat head screws on the dedicated screw slot present on mounting bracket.
-
Hang the RS485 converter on the two M3 x 6 mm flat head screws installed on the mounting bracket.
-
Install the LoRa connector on the mounting bracket with two M4 x 25 mm self tapping screws.
-
Tighten the screws using PH1 screwdriver.
Cellular Configuration:
| NOTICE |
|---|
|
REDUCED DEVICE PERFORMANCE
Failure to follow these instructions can result in equipment damage.
|
-
In case of a cellular configuration, open the four screws on the sides of the Flex-Server and carefully open the box, without removing the antenna cables. Insert a micro-SIM card and close the Flex-Server.
-
Attach the Wi-Fi antenna to the Wi-Fi antenna connector on Flex-Server.
-
Attach the 4G antenna to the 4G antenna connector on Flex-Server.
-
Slide the Flex-Server on the mounting bracket.
-
The new power supply has + and -ve to be connected to the Flex-Server’s +ve and -ve.
-
Connect the Modbus or the BACnet to the RS485 port on the Flex-Server.
-
Connect Modbus or the BACnet to the RS485 converter using the manual provided with the RS485 converter.
-
Connect the LoRa module using the USB cable provided in the box.
-
Connect the RS485 converter with the USB cable provided in the box.
-
Plug the Power Supply Adaptor.
-
Switch on the AC mains power supply.