DOCA0343EN-03

Introduction

EcoStruxure Master Range

EcoStruxure™ is Schneider Electric’s IoT-enabled, plug-and-play, open, interoperable architecture, platform, and buildings. Innovation at every level from connected products to edge control, and applications, analytics, and services.

Overview

EcoStruxure Flex-Server is a multi-protocol IoT gateway that has been designed specifically for commercial applications. It enables businesses to perform bi-directional data or control communication between a range of sensors and devices on-premises and cloud. Exposed physical interfaces include RS485, USB ports, power connector, LEDs, and Ethernet.

System Features and Benefits

The features and benefits of Industrial or Commercial grade Flex-Server are:

  • Running standard Linux operating system.

  • Fanless operation.

  • Remote bidirectional connectivity between cloud and Flex-Server over a VPN.

  • Remotely manage all gateways from a single portal.

  • Role-based access control for Flex-Server management for different users.

  • Remotely configure connected devices on the Flex-Server over the supported protocols.

  • Pre-supported library of hundreds of devices.

  • Remote health monitoring and management.

Supported Gateways

The supported gateways are listed below:

  • LoRa connector - RAK Wireless 7371 - D10005

Box Contents

The box contains the listed parts:

  • EcoStruxure Flex-Server IoT gateway

  • Power supply

  • 4G antenna

  • Wi-Fi antenna

  • Four M3 x 6 mm screws flat head

  • Four M4 x 25 mm self-tapping screws

  • Installation guide

  • Mounting Bracket for Flex-Server

  • Mounting bracket for LoRa and RS485

Architecture

The sample architecture of the EcoStruxure Flex-Server is shown in the following diagram:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.