LED Indicators
LED indicators are used to check the status of the internet connection, server connection, SD card health, Flex-Server firmware health, device connection, and data transfer. Refer to the below tables for more details about top LED indicators and bottom LED indicators.
Flex-Server Status LED
Network Status LED
Ethernet Status LED
|
Sl. No. |
Indicator |
Description |
|
1 |
Ethernet communication is not connected. |
|
|
2 |
Ethernet LED 1: |
Ethernet communication active. |
|
3 |
Ethernet LED 2: |
Ethernet communication active. |