DUG_SmartDim LED Puck Multiwire_WH-01

About the document

Document Scope

This document provides comprehensive guidance on the ELKO - SmartDim LED Puck Multiwire, detailing its features, installation, configuration, and operation. It explains how to pair the device with the Wiser Hub, adjust brightness levels, and use the Wiser Home app for control and automation. Users can create schedules, assign device locations, and configure connected switches for personalized lighting experiences. The document also covers pairing multiple pucks, setting dimming modes, and managing device behavior through app-based settings and manual controls.

Validity Note

The characteristics of the products described in this document are intended to match the characteristics that are available on www.elko.no. As part of our corporate strategy for constant improvement, we may revise the content over time to enhance clarity and accuracy. If you see a difference between the characteristics in this document and the characteristics on www.elko.no, consider www.elko.no to contain the latest information.

For your safety

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Safe electrical installation must be carried out only by skilled professionals. Skilled professionals must prove profound knowledge in the following areas:
- Connecting to installation networks.
- Connecting several electrical devices.
- Laying electric cables.
- Safety standards, local wiring rules and regulations.
Failure to follow these instructions will result in death or serious injury.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
- Make sure that the terminal connection area does not come in contact with the metallic parts of any device installed in the same location.
-Do not short the outputs to neutral.
Failure to follow these instructions will result in death or serious injury.
NOTICE
HAZARD OF EQUIPMENT damage
- Always operate the product in compliance with the specified technical data.
- Never connect any mixed inductive/capacitive loads.
- Connect only dimmable loads.
- Do not use dimmable socket outlets.
- Ensure that the device is disconnected from its circuit during the insulation resistance test.
Failure to follow these instructions can result in equipment damage.

General Cybersecurity Information

In recent years, the growing number of networked machines and production plants has seen a corresponding increase in the potential for cyber threats, such as unauthorized access, data breaches, and operational disruptions. You must, therefore, consider all possible cybersecurity measures to help protect assets and systems against such threats.

To help keep your Schneider Electric products secure and protected, it is in your best interest to implement the cybersecurity best practices as described in the Cybersecurity Best Practices document.

Schneider Electric provides additional information and assistance:

Environmental Data

Find and download comprehensive environmental data about your products, including RoHS compliance and REACH declarations as well as Product Environmental Profile (PEP), End-of-Life instructions (EOLI) and much more.


https://www.se.com/myschneider

General information about Schneider Environmental Data Program

Click the link below to read about Schneider Electric’s Environmental Data Program.


https://www.se.com/ww/en/about-us/sustainability/environmental-data-program/

Declaration of Conformity

Hereby, Schneider Electric Industries SAS, declares that this product is in compliance with the essential requirements and other relevant provisions of RADIO EQUIPMENT DIRECTIVE 2014/53/EU.

Declaration of conformity can be downloaded on:

Available Languages of the Document

The document is available in these languages:

  • English

  • Norwegian

Information on Non-Inclusive or Insensitive Terminology

As a responsible, inclusive company, Schneider Electric is constantly updating its communications and products that contain non-inclusive or insensitive terminology. However, despite these efforts, our content may still contain terms that are deemed inappropriate by some customers.

Trademarks

  • Wiser™ is a trademark and the property of Schneider Electric, its subsidiaries and affiliated companies.
  • Zigbee® is a registered trademark of the Connectivity Standards Alliance.
  • Apple® and App Store® are brand names or registered trademarks of Apple Inc.
  • Google Play™ Store and Android™ are brand names or registered trademarks of Google Inc.
  • Wi-Fi® is a registered trademark of Wi-Fi Alliance®.
  • QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Other brands and registered trademarks are the property of their respective owners.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.