DUG_SmartDim LED Puck Multiwire_WH-01

Removing the device from Wiser system

Using the Wiser app, you can remove the Puck from the system.
  1. On the Home screen, tap .
  2. Tap Devices > Micromodule Dimmer > Delete (A).

    NOTE:
    • Removing the device will reset the Puck. After reset the LED turns amber indicating that the Puck is ready to pair with another network.

    • If there is a problem while pairing or resetting the Puck, refer to Resetting the device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.