DUG_SmartDim LED Puck Multiwire_WH-01

Testing the device

Before using the Puck, manually test it and make sure that it works when connected to the lighting devices.

WARNING
HAZARD OF ELECTRIC SHOCK
  • Observe the regulations for working on live parts.
  • Only actuate the device buttons using insulated auxiliary equipment that meets the requirements of EN 60900.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

  • Short press the Set (Setup/Reset) button once, the connected lighting device turns on/off.

  • Press and hold the Set (Setup/Reset) button to adjust the dimming level of the connected lighting device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.